Hi team,
my customer is using J6/913/914.And meet below questions:
We checked the frame of camera data in J6, and it shows as the black image, while in normal it will show as captured picture.
So there are some questions about this phenomenon that:
- From camera to TI913: Is there any method rather than make sure that the data from camera to TI913 is correct?
- From TI914 to J6: How can we make sure this channel is working well during running time?
- For TI914: how can we make sure that there is nothing wrong with TI914 in this situation?
Please share some suggestions with us from the point of view of TI914. Thanks.
BRs
Given