Part Number: TIOL111
Hello,
As TIOL111 works as level shifter which takes care physical link and voltage translation from 24 V to 3.3 V and vice versa. I am clear that master's 24 V is converted to device's 3.3 V required for controller but I do not get how this TIOL111 IC converts 3.3 V from controller to 24 V output required for IO link master. Does this IC alone can level shift or any external pull up is required.
I came up with question because controller can give output -> 3.3 V and maximum 20mA with just this much how TIOL111 can step up the voltage upto 24V and how much will be current ?