Hi Sir/Mam,
I am Embedded engineer i have experience in working with the bluetooth low energy based applications. Recently i came across a requirement to design an active usb cable for USB 2.0. I have done my research in order to find which shall be suitable redrivers for my application and i came across the following options TUSB213, TUSB215, TUSB217. I feel that the TUSB217 is great but unfortunately the client doesn't wish to have a costly product.
The client wants to design an active cable of 10m. I have read across the forum that the TUSB213, TUSB215 supports 5m pre channel and 2m post channel cable length.Though i have read the meaning of pre channel and post channel still i dont understand why the TUSB213 and TUSB 215 has only 2m post channel cable length when the description data in the product selection window shows 4m cable length support. It will be great if anyone can let me know what shall be maximum post channel cable length support for TUSB213 and TUS215 assuming good quality usb cable.
I hope that TUSB213 and TUSB215 shall support atleast 5m of post channel cable length because as per my research i have also came across many 10m cables which are made using two redrivers.
Please let me know which shall be best redriver for my requirement. Thanks
Regards
Piyush Saxena