Part Number: TCAN1043G-Q1
Other Parts Discussed in Thread: TCAN1043
Hi Team,
two questions on TCAN1043.
1. if VIO and Vcc are connected together, do you think we can just use 1x100nf totally? datasheet mentioned 1x100nf on each pin.
2. as you recommended in e2e, WAKE is connected to Vsup if not used, rather than connect to GND. So if WAKE pin is connected to Vsup, since its internal circuit is also connected to Vsup, then no leakage current consumption, right ?
3. as you mentioned in e2e, on TJA1043, there is SPILT pin which need connect to a cap. And our part is not needed. But if NC pin is connected to a cap, will it bring negative effect?
Thanks.