Part Number: SN75DP128A
Hello team,
I have a customer asking some questions on the SN75DP128A.
1. Do we have any reference schematics for this device? i did not see an EVM on ti.com, did i miss something?
2. What length of DP can this device drive? min/max (under what conditions)
3. one of the DP output is connected to a Serializer on the same board, and the other one is external - would this cause a problem? Can one throttle the internally connected DP to not drive it as much and drive the 2nd channel (external) more? - In general any concerns with connecting to an internal/local DP connection with this device?
Thanks! Appreciate the support.
Best,
Saqib Mohammad