This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041A: About Unused pins at USB2.0 only

Guru 21045 points

Part Number: TUSB8041A

Hi Team,

 

We use TUSB8041A at USB2.0 only (don’t use USB3.0 signals).

Then, we guess that the following(Unused) pins is floating.

Is my understanding correct?

If no, could you please let us know the suitable connect (GND or Other power rails)?

 

[Unused pins]

USB_SSTXP_DN3 (19pin)

USB_SSTXM_DN3 (20pin)

USB_SSRXP_DN3 (22pin)

USB_SSRXM_DN3 (23pin)

USB_SSTXP_DN4 (26pin)

USB_SSTXM_DN4 (27pin)

USB_SSRXP_DN4 (29pin)

USB_SSRXM_DN4 (30pin)

 

Regards,

Kanemaru