Part Number: TCA6424
Dear Team,
The problem currently encountered in this application is that the IO Pin is easily short-circuited when hot plugging (300kΩ high impedance becomes 130Ω)
Even if IO Pin is not dead, it's Pull High's impedance will be lower and lower (300kΩ==>60kΩ).
There are already TVS and Spike prevention solutions on every IO line.
Do you have any suggestion to solve it?
BR
Kevin