Part Number: TCA9554
Dear,
Using TCA9544, 2V power supply, and our customer find that why the INT couldn't pull up to high level and stay 0.9V with 10Kohm pull up resistor? When changed to 1K, it is normally.
According to the source current of datasheet, we could caculate the resistor value about 1K, and the datasheet recommend 4.7Kohm. I think the rise time should be slower but could get to high level if connect to 10Kohm, but now it stay 0.9V, please give me some advice?
Best regards
Kailyn