Part Number: TUSB9261-Q1
A minimum flash size of 512 kbits (64 k x 8) is recommended, but please be aware of any disadvantages in electrical performance when selecting a SFLASH with a larger capacity.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261-Q1
A minimum flash size of 512 kbits (64 k x 8) is recommended, but please be aware of any disadvantages in electrical performance when selecting a SFLASH with a larger capacity.
Hello,
So long as the flash satisfies the minimum requirements of 64k x 8, any larger sized flashes should work. The flash burner utility will just leave the addresses above blank. Just do not increase the bit width of the flash, eg a 512kbit flash that is 32k x 16.
Best,
Gerasimos