This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044: dip switch configuration for standard use, without any 12c eeprom or smbus options

Part Number: TUSB8044


Goodmorning, if i want to avoid using the eeprom and any other smbus, i2c communication protocol, which is the I/O configuration to adopt?

I saw the evaluation board, but there are the dip switches on the board, and it is not specify in which configuration they should be. For example, for an individual port power control and a single port overcurrent input mode, which configuration should i use? it's not very clear on the documentation.

thanks in advance