Part Number: LMH0318
Other Parts Discussed in Thread: USB2ANY
I have an SDI signal at 1.483Gbps going through a cable equalizer and into the LMH0318. The input signal, as measured on a Phabrix SX has 0.12UI jitter at 100kHz. The output signal from the reclocker has 0.14UI jitter at 100kHz and the rise times and fall times are longer. The status registers say it has locked onto the input, and that the CDR is working, but it doesn't seem to do it's job. I have tried different EQ settings, different signal drive strength settings (these do change the overall amplitude of the waveform, so clearly we are controlling the LMH0318), but I cannot get a proper eye opening on the output or get any jitter removed - at the moment it seems to be adding to it.
Regards,
Simon