This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: Spec of VDD33 VDDIO rise time

Part Number: DS90UB948-Q1

Hi team,

The rise time of VDD33, VDD12, VDDIO in DS90UB948-Q1 datasheet has been chagned from the datasheet's 2016 version as below.

Old datasheet spec     -> VDD33, VDDIO < 1.5ms (max)

New datasheet spec   ->  0.2ms (min) <  VDD33, VDDIO

BTW, the rise time of VDD33, VDDIO in a customer's board is measured with 100us. The rise time is violated with new datasheet spec even though it was okay in the old one.

-. Is it okay or not? What is the expected problem?

-. Can you explain why the spec has been changed?

Thanks,

Sam Lee