Hi,
In table6, page21 of 953 spec, there is a CSI bandwidth. For example, when 953 in my design is using sync.mode and Reference frequency is 26MHz, the CSI bandwidth is 26x128=3.328Gbps. My question is, does this bandwidth include MIPI CLK lane? If I am using a 4 data lane camera, what is the max. bandwidth of each lane? 3.328/4=832Mbps or 3.328/5=665.6Mbps?
If MIPI CLK is not transmitting in forward channel, does it recover at 954 and output together with other 4 data lane?
Thank you and look forward to hearing from you soon.
/Sen