This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: SGMII 4-Wire Connections

Part Number: DP83867IS

Hi all

Would you mind if we ask DP83867IS?
We consider using SGMII 4-Wire connections with DP83867IS.
We would like to confirm the termination of unsed pin.

-TX_D2/TX_D3 : Open or pull-down with 1kohm?
-TX_CTRL : Open or pull-down with 1kohm?
-RX_D2(SGMII_SOP)/RX_D3(SGMII_SON) : AC coupling with 50ohm GND(please refer to follows) or open?
  
Could you give us the advice?

Kind regards,

Hirotaka Matsumoto