Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB953-Q1
We are having some data transport issues between the FPD Link serialiser and de-serialiser ICs (DS90UB953-Q1, DS90UB954-Q1) where video frames are lost when the connecting cable is trodden on. To try and see what is happening to the actual signal when the cable is stepped on, I wish to view the eye diagram of the signal as it arrives at the deserialiser IC using a high performance scope. The problem is that the back-channel data being ‘overlaid’ onto the 4Gbps data makes it almost impossible to take an eye diagram on a high speed scope as the signal is jumping up and down with the back channel data as it is sourced from the deserialiser back to the serialiser.
So is there anyway of disabling the back-channel data or any other way you can recommend whereby we can observe the eye-diagram of the incoming signal at the deserialiser pins (or probably more accurately, across the DC blocking caps)?