Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, LM5175
Hi ,
I have TPS65987 on board configured as sink . I generate a program that works on TPS65987 EVM. The only difference between our board and EVM is that PHV1 is floating - on EVM it is connected to SYS_PWR. I changed the ADCIN1 to resistor ratio to 0.24 which is BP_WaitFor3V3_Internal and safe configuration. In Debug mode of TPS65987 Application customization tool I see PD negotiated on EVM but when I connect to our board there is no negtiation. Is it because PHV1 is floating on our design.
Regards,
Ali