Other Parts Discussed in Thread: BQ24610,
Dear TI,
I use BQ24610 to charge singe Li-ion battery(3.0V~4.2V Full charge ), and set my device as sink / UFP,
Set 2 sink PDOs,
1. 5V/3A
2. 9V/3A
1.if Battery voltage > 3.8V, open my device and plug USB-C adapter ,then TPS65987D VBUS=9V ,PV_HV1= 8.98V to BQ24610 , and start to charge battery.
2.if Battery voltage < 3.7V, open my device and plug USB-C adapter ,then TPS65987D VBUS=5V, PV_HV1= 3.1~3.7V to BQ24610 , and it can't charge battery.
could you help to check it, does there have any setting should be modified from TPS6598X Application customization tool or USB PD circuit?
Thank you very much for your help.