Part Number: TUSB4041I
Hi Team,
My customer is looking for the TUSB4041I Windows 10 Driver. He told me that Win10 could not get it automatically when he uses the device TUSB4041I.
Regards,
-Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Hi Team,
My customer is looking for the TUSB4041I Windows 10 Driver. He told me that Win10 could not get it automatically when he uses the device TUSB4041I.
Regards,
-Renan
Hello Renan,
You do not need need a specific driver for TUSB4041. It should work when plugged into a windows 10 machine. It may be an issue with your circuit or with your generic USB hub driver in windows.
Best,
Gerasimos
Alexey Tyutin said:Is it possible that 1uF cap on GRSTz is not enough if I apply 3.3V and 1.1V simultaniously?
My bad, first comes 3.3V, then after 600ms 1.1V.
Shorting GRSTz cap wit tweezers has no effect.
Removing the resistor from smbus clk (R74) gave an effect: now I see 2 downstream usb ports.
It is working correctly now.