Part Number: DS90UB936-Q1
Hi TI,
Is each RIN channel of DS90UB936 can transfer 3Gbps data rate?or the total capabilty(RIN0+RIN1)is 3Gbps?
Can we connect two ds90ub935(each RIN channel connect one) to one DS90UB936?
BR
Jason Koo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB936-Q1
Hi TI,
Is each RIN channel of DS90UB936 can transfer 3Gbps data rate?or the total capabilty(RIN0+RIN1)is 3Gbps?
Can we connect two ds90ub935(each RIN channel connect one) to one DS90UB936?
BR
Jason Koo
Hello Jason,
yes the 936 can be connected to 2x 935 at the same time. Each link supports up to 3Gbps.
Hi Hamzeh,
Tkanks for your reply, another question is for the case(2x 935 at the same time) how sholud we config the mipi output?
like 1. CLK0+DATA lane0,1 for RIN0, CLK1+data lane2,3 for RIN1
2. CLK0+DATA lane0,1,2,3
is there any concern?
BR
jason koo
Hello Jason,
in the 936 you can't devide the output lanes per input port. You have only option #2 you mentioned.
Hi Hamzeh,
Does the DS90UB954 can devide the output lanes per input port?
BR
Jason Koo
unfortunately Not.
You can use the 960 if you want each camera at a seperate MIPI output.