Part Number: DP83822IF
Other Parts Discussed in Thread: DP83822HF, TIDA-00928
Hi:
I have several question regarding for DP83822 .
i> the latest Dp83822hf datasheet 2019 verdion, both of VDDIO and AVD can use 1.8V , whle old version for AVD can only use 3.3V , how can I choise the AVD .
ii>I use TIDA-00928 reference to desing the 83822,I want to use 100base-FX mode with AFBR5803z model , regarding for COL signal bootstrap, from the bootstrap table , should config with mode 2, or 3, but in TIDA-00928 which connect to GND with 2.2K parellar with 470 ohm and LED , if this config ok ? what is the meaning for LED ?
iii>when config RX-ER with 13K and 1.96K , the LED_1 will as signal detection and is active LOW ,it is digical signal , but AFBR 5803 SD output is PECL , if it is can direct drive 83822 LED_1.
regard
Jonathan