Part Number: DS90UH927QEVM
Dear TI Team:
I got a trouble that there is no any LVDS signals output in Deserializer 928 board.
The following are my platform setup.
1. Serializer 927 are paired with Deserializer 928 with FPD-Link III cable.
2. I can talk Deserializer 928 registers by Serializer 927.
3. I can set 927 to enable Pattern generator mode and Deserializer 928 can normally output LVDS to driver display, this is no problem.
4. When I disable Serializer 927 pattern generator mode and signals source is form external LVDS channels. But Deserializer 928 has no any response from 927 LVDS signals.
I have some questions would like TI can support me to clarify.
a. Once 927 & 928 are paired with successful. And I followed TI normal registers setting. If LVDS input to 927, should Deserializer 928 have LVDS output from 927?
b. If the answer is yes, do I miss something? or have to set some registers to enable something?
Looking forward to your feedback.