Part Number: TUSB4041I
Dear TI-Support,
i am trying to figure out if the TUSB4041 is causing a problem in our system.
The system consists of a host PC and a daughter card connected through a backplane.
On the daughter card we designed the TUSB4041 to be self-powered, i.e. the TUSB4041 remains in-active as long as the daughter cards power switch isn't turned on.
The observed failure is as follows:
When the daughter card is switched on, sometimes the USB device tree in Windows disappears and all USB peripherals are no longer available.
The data lines between host PC and TUSB4041 are permanently connected, even during GRSTz = 0.
We guess that during this state the host PC may be sending data causing problems.
The host PC may detect a short-circuit event by mistake and switches off its USB controller.
My questions are ...
Related to the USB2.0 specification may the data lines be permanently connected to each other?
I could not find anything in the specification or i am still missing it.
Which state do the differential transceiver have during GRSTz asserted low? High-Z?
Do you recommend to set AUTOENz/HS_SUSPEND = 0?
Thank you in advance.
Regards,
Christopher