Part Number: DS90UH927QEVM
Dear TI Team:
I had a trouble about Deserializer 928 in Pattern Generator mode no working.
The followings are my platform setup:
1. Serializer 927EVM board paired with Deserializer 928 by FPD-Link III cable.
2. I used my MCU board and connected 927EVM by I2C channel.
3. I can talk all ICs and program registers for every ICs which are on I2C bus.
4. When I set 927EVM to enter Pattern Generator mode, Deserializer 928 can output LVDS signals to display.
5. But when I set Deserializer 928 to enter Pattern Generator mode. Deserializer 928 cannot work and cannot be talked by 927EVM. The following are my setting to 928.
0x02=F0h; 0x03=7Ch; 0x1C=03h; 0x24=00h; 0x29=07h; 0x39=02h; 0x64=31h; 0x65=05h;
I have 3 questions:
a. Is it not correct that I set Deserializer 928 register?
b. Based on the platform, can I enable Deserializer 928 to enter Pattern Generator mode in 927EVM side?
c. If yes and 928 can enter pattern generator mode, at this moment, once I remove FPD-link III cable but power is still keeping, can the Deserializer 928 still be working?
Looking forward to your feedback.