Part Number: SN75HVD05
Other Parts Discussed in Thread: PROFIBUS, SN65HVD20, THVD1450
Hi,
Our customer are planning to use RS485 driver SN75HVD05D.
They have question about SG(Signal Ground).
In common case, RS485 cables all nodes using differential signals (+/-) and
as well as SG, three wires in total.
But in their end customer's system, it is using the cable which have only two wires.
In this case, it is necessary to stop the explicit connection of SG to the cable and
take measures to match the SG level of each RS485 circuit as an alternative.
(Their cable length is up to 350 meter)
We understood that two wire connection is not the common use case in RS485,
but we need to use two wire cable, so if you have any example circuit of RS485 to use 2 wire cable,
could you please give us an advise?
For reference, PROFIBUS seems to have an example to handle with 2 wires.
In that case, it seems that SG of each RS485 circuit is loosely grounded with high resistance of mega ohm to match the SG of each 485 circuit while suppressing the influence of GPD.
It would be nice if you could also give us the 2-wire experience with TI products.
best regards,
g.f.