Part Number: DP83822I
Hi Team,
We desinged in DP83822I in a BT speaker application. Could you please help to review below schematic and let me know if you have any concerns? It is working at RGMII mode. Thanks.
Regards,
Nic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hi Team,
We desinged in DP83822I in a BT speaker application. Could you please help to review below schematic and let me know if you have any concerns? It is working at RGMII mode. Thanks.
Regards,
Nic
Hi Nic,
I can have the schematic reviewed by early next week.
-Regards
Aniruddha
Hi Nic,
Following are some comments on the schematics,
Magnetics connection needs to match the datasheet figure 33. I do not see decoupling capacitors on center taps. center taps should also be pulled up to AVDD.
49.9ohms resistors should be placed close to the device.
RBIAS resistor should be 1% tolerance
25MHz input clock should meet the datasheet requirement.
In mode 2 strap on RX_ER pin, Auto MDIX will be disabled. Check if this is a requirement for the system.
33ohm series termination resistors can be replaced by 0ohm. DP83822 has internal termination resistors.
-Regards
Aniruddha