Part Number: TCA9539
Hi,
In the data sheet chapter 9.2.1.2 there is mentioning that in order to minimize ICC when driving LED parallel resistor of 100kohm can be used.
Looking at graph Fig18 , it looks like for Vi=Vcc-0.6V the additional Icc is around 5.5uA at 35C and Vcc=3.3V
Adding 100kohm creates additiona current when LED is on of 33uA. It looks like the remedy is worse than current we can expect when Vi =3.3V-1.2 V= roughly 12uA.
Is it right to interprete this fix as valid only for situation when LED is off for majority of time?
Is my estimate of additional current when Vi =Vcc-1.2V being roghly 12uA at 35C , Vcc=3.3V correct?
The second fix is to drive LED from higher voltage and example shows 5V LED VCC and 3.3V VCC. In this case if both voltages are not powering up simultaneousy the TCA9539 can be backdriven from 5V until 3.3 V settles , is this device ok with this situation?
Regards
Sebastian