Part Number: TPS65981EVM
Other Parts Discussed in Thread: TPS65981
Dear TI friends
, I'm studying module TPS65981EVM and have a question need you help.
I have:
+ one TEA1936XDB1475: Multi Standard 27W Mobile Charging
+ and one TPS65981EVM USB Type-C™ and USB PD controller
I want to use TPS65981EVM like a Load for test output voltage of TEA1936XDB1475, but I don't know how to connect them.
As I know TEA1936XDB1475 has some lever output: 5V, 3A or 9V, 3A or 12V, 2.25A ...... output voltage depend on IC Type output TEA19051.
And When I use TPS65981EVM as a Load, I don't know how to connect.
Please help to guide me connect them, after that I can test all level output of TEA1936XDB1475
Thank and best regards !