Part Number: DP83825I
Hi Expert,
I have question about DP83825i. The LED0 and LED2 are all strap pins. Does customer need configure the strap status of these pin first and then consider to use which structure external circuit for the LED?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83825I
Hi Expert,
I have question about DP83825i. The LED0 and LED2 are all strap pins. Does customer need configure the strap status of these pin first and then consider to use which structure external circuit for the LED?
Hi Lenna,
Yes, since the LED pins are also strap pins the external LED circuit will change based on strap configuration. First customer should decide which strap they are going to use on the LED pins and then connect the LED circuit accordingly.
-Regards
Aniruddha