Part Number: DP83848I
Hi,
We are designing a communication bridge device based on the MCU MC68360 from NXP and a TI based Ethernet controller DP83848I.We are using SNI interface for the same. But when we look into the CLK duty cycles requirement The TX CLK duty cycle of DP83848I is 25ns,75ns ( TCLK width Low, TCLK width High) whereas in our processor , MC68360 it is required as (45ns ,40ns) min. So do you have any option to change the duty cycle of TX CLK to( 50ns,50ns)? We are not sure whether we can go ahead with our design.Could you please confirm on this?