Part Number: TUSB211
Other Parts Discussed in Thread: TUSB213
Hi there,
Could you please give comments about the question from our customer below?
1.TUSB211 does not need to disconnect the USB cable when doing SI redriver. This shows that the TUSB211 compensates the USB bus in a certain way. Which part of the bus does the TUSB211 mainly compensate?
2. TUSB211 is hung on the bus. Strictly speaking, it increases the load of the bus. How to adjust the SI bus because of the excessive capacitance load?
3. What is the difference between TUSB211 and TUSB213?
4. In the picture below, the first half of the eye is pressed down and the second half is normal. What is the cause of this phenomenon?

5. When the eye diagram is divergent, can the TUSB211 function to close the divergent waveform (as shown below)?
Thanks!
Eason