Part Number: TPD4E05U06
Hi Champs,
do you see any issues using the TPD4E05U06 for two independent USB 2.0 480Mbps channels?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD4E05U06
Hi Champs,
do you see any issues using the TPD4E05U06 for two independent USB 2.0 480Mbps channels?
Hello,
There is no issue doing this. The device will protect both as intended
Hi,
thanks for the fast answer!
Do you expect a crosstalk between two different USB channels within one housing (TPD4E05U06)?
Kind regards
Simon Fischler
We have the S-parameter available for the part that will give you the cross talk between channels of the device. It only shows the cross talk between two channels but this is true for each of the channels of the deivce.