Part Number: DS90UB960-Q1
Hi,
I have setup as shown on image below. I'm using Leoni Dacar coax cable to connect two boards. When using longer cable (~ 5 m), the link is very stable, but when using short cable (0.5 - 1 m) the link is completely unstable, pass/lock signals are not stable. So, my question is how I can make it work stable with any cable length (up to 5 m). Adaptive EQ is enabled and 0xD5 value is set to 0xF3. Registers 0xD2 - 0xD4 have their default values.
Can you help me with this problem with some suggestions or tips?
Best regards,
Stefan.