Part Number: TUSB7340
I could not find how to change drive strength of PCIE_TX.
Can I change drive strength or slew rate?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB7340
I could not find how to change drive strength of PCIE_TX.
Can I change drive strength or slew rate?
Please refer to section 7.3.1.1, you can change output SWING and De-emphasis through the De-Emphasis and Swing Control Register.
Thanks
David
Hi avid
I knew these parameters. I took these parameters as ethernet lines.
Are these really related to PCIE lines?
I'm asking for PCIE_TX lines, connected to micro-processor.
Regards,
Unfortunately, the control is only provided on the USB side, not on the PCIe side.
Thanks
David