Part Number: TPS25810
Hi Sir,
Would you please help to check the schematic to see is any problem if want to design TYPE_C_3A solution.
Beside, Is any thing need to consider in layout or others.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25810
Hi Sir,
Would you please help to check the schematic to see is any problem if want to design TYPE_C_3A solution.
Beside, Is any thing need to consider in layout or others.
Hello,
Remove the 5.1k ohm resistor connected to CC2 (R6). This would cause for the TPS25810 to detect that a device has been connected even though nothing is connected, forcing 5V continuously on VBUS which breaks the Type-C spec. As far as layout recommendations, I would follow the layout guidelines induced within the datasheet (section 10).