This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1450: VCC and Absolute max for bus voltage

Genius 17855 points

Part Number: THVD1450
Other Parts Discussed in Thread: SN65HVD3088E,

Hello,

I have a question for VCC and absolute max relationship of THVD1450 and SN65HVD3088E.

Both SN65HVD3088E and THVD1450 specify certain absolute voltage range that does NOT depend on VCC voltage for Bus Voltage(A,B,Y and Z) absolute max.
It is -9 - +10V for 3088E and it is -18 - +18v for THVD1450.

Does it mean both devices are not damaged with bus voltage being within this range even if VCC is not powered?

Regards,
Oba