Part Number: THVD1550
Other Parts Discussed in Thread: TIDA-01401,
Hi team,
My customer has some problems about TIDA-01401 as below.
1.About the description in Page 7.
(1)using R42//R43 with 470pF as a low pass filter to improve the immunity?
(2)using R42+R43 with 220pF as a low pass filter to improve the immunity?
(3)Both (1)+(2) are used or just one of them is enough?
(4)Why 220pF and 470pF are used in this case, how to calculate, determined by cutoff frequency? R42/43 is 59Ohm, it is for terminal impedance match?
2.About EFT test result of Fig.23 and Fig.25.
It seems the result of Fig.25 is worse after using the same transceiver. Does it mean our TIDA board is worse than the unknown encoder? How to understand?
If customer want to improve the EFT performance, what method could be used?
Thanks.
Robin