Part Number: SN65LVELT23
Hi,
I understand that VIH, VIL and VIHCMR are the voltage levels in the following figure.
Is it correct?
Best regards,
Yuto Sakai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVELT23
Hi,
I understand that VIH, VIL and VIHCMR are the voltage levels in the following figure.
Is it correct?
Best regards,
Yuto Sakai
Yuto-san
The diagram is correct. The two important parameters are the VPP and VIHCMR, please make sure the input signal can met these two requirements.
Thanks
David
Hi David-san,
Thank you for your reply.
I would like to ask additional questions.
I do not understand what the definition of VIHCMR.
I believe that VIHCMR is the middle value of the differential input signal, and is the range 1.2 to Vcc,is it correct?
And, I understand that it is necessary to input a signal that keeps the input swing within VPP,is it correct?
Best regards,
Yuto Sakai
Yuto-san
VIHCMR min is 1.2V and max is 3.3V. The common mode range places an upper and lower boundary on the differential high input level.
The input signal swing has to be with in the VPP range.
Thanks
David
Hi David-san,
Thank you for your reply.
Does it mean that VIH and VIL are just measurement data and not the definition of range?
How is the upper and lower limits determined by VIHCMR?
Best regards,
Yuto Sakai
Yuto-san
VIHCMR lower and upper limit is determined by the device type.
The differential signal levels are specified as Vpp and VIHCMR, these are the two parameters that need to be met.
Thanks
David