Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9539, , TCA8418E, TCA8418
hello
I want to use this device to detect the activity on communication line. When the communication is not active, the line is fixed to low. when the communication started, the line will go high and low, continuously switching. The TCA9539's /INT will go low when the state of input pin changed, but it will also go high when the input pin state change back to original value. I want to latch this /INT low when the communication started.
Is there any good idea to do this? any recommendation?
I will use remaining input port for DC level detection and send interrupt to MCU.