This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: DS90UB936-Q1 device address

Part Number: DS90UB936-Q1


My camera uses AR0144, its internal integration TI 935, I connect to 936 development board through harness, and then connect to s32v through Mipi interface. How many device addresses can I find on I2C bus after hardware connection?

Now I can only find a 936 I2C device address 0x30, is it necessary to configure 936 to see the address of 935 and camera? Or is there something wrong with my hardware board?

  • Hello Meng,

    It sounds like your devices aren’t properly linked. Once linked, you should see device addresses for the 935/936 and camera.

    To check your link, you need to verify the aliases by doing the following:

    - Des Reg 0x4C: Select the right RX port to write
    - Set/Check real I2C addresses
    - Reg 0x5B SER DEVICE ID: Set the real serializer I2C address. This is typically loaded already
    - Reg 0x5D SlaveID[0]: Set the real CMOS sensor I2C address
    - Reg 0x5C SER_ALIAS_ID: Set the alias serializer I2C address
    - Reg 0x65 SLAVE_ALIAS_ID[0] (camera alias ID): Set the alias CMOS sensor I2C address

    Once the aliases are set, you can communicate with the 935 using the alias ID’s that you assigned.

    Best,

    Liban H.