Part Number: DS8921
The datasheet lists max ICC (35 mA) but not a nominal.
If the devices runs at max ICC, the power dissipation is 175 mW (35 mA * 5 V). At 85C, the part is rated for 172 mW (730 mW - [(9.3 mW/C)*(85C-25C)]) however the DS8931ATM is rated up to 85C. If the 9.3 mW/C derating is correct and the device is running at max ICC, how can the part operate at 85C? Is the derating correct?
Thank you.