This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD224: Is there any side effect when used for 3.3V LVCMOS pin ?

Guru 19785 points

Part Number: ESD224

Hi Team,

I would like to confirm if ESD224 could be used for 3.3V LVCMOS input pin.

Regarding the block diagram, I believe each pin are independent, so there should be no problem as long as the device input voltage does not exceed the recommended operating range of 3.6V.

If there is any limitation for this use case, please let us know.

Best Regards,

Kawai