Part Number: DS90UB948-Q1
Hi E2E members,
Is it possible to pass YUV422 as a data transmission path with the combination of DS90UB947 or DS90UB927 and DS90UB948?
As a premise, openLDI does not have a public data array for transmitting YUV422.
For example, the data array on openLDI is determined between the image sensor connected to the serializer and the imager connected to the deserializer.
H, V and DE are embedded in the data as well as RGB.
The DS90UB9x7 and DS90UB948 don't distinguish between YUV422 and RGB888 data, so I think they can pass it. Is this idea correct?