Part Number: DS90UB960-Q1
Is VC-IDfeature compatible with MAX9295?
Take the following example:
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Is VC-IDfeature compatible with MAX9295?
Take the following example:
Thank you!
Hello,
the UB960 output ports are MIPI DPHY Version 1.2 / CSI-2 Version 1.3 Compliant. If the Maxim component has MIPI CSI input which is compliant with the same standard, then yes you can use it in this way.
But I would recommend you use the DS90UB953 Serializer at this position instead of Maxim component.