Part Number: DS90UB953A-Q1
Other Parts Discussed in Thread: DS90UB954-Q1
For our industrial imaging application, we are considering using the DS90UB953A-Q1 serializer and DS90UB954-Q1 deserializer to support multiple image sensors. The full frame output of the sensors will exceed 1920Hx1080V pixels, output over a CSI-2 interface in various RAW formats at up to 60fps. The application will configure the sensors for various non-standard partial frame outputs that output only a sub-rectangle from the full sensor.
My questions, without having fully read the 953 data sheet, concern the supported video formats.
The data sheet states that the 953/954 support 1920Hx1080B at 60fps in RAW formats. Does this represent the upper limit of the channel capacity?
Do the serializer and deserializer require different configurations for different video formats?
Do the serializer and deserializer support only standard video formats, or will they support unusual (non-standard) horizontal and vertical resolutions in RAW modes that output only a sub-rectangle from the full sensor?
If so, then is the frame rate limited simply by the SerDes channel capacity, or are there further limitations that depend on the video format? In other words, will selecting a sub-rectangle from the full sensor allow us to achieve a greater frame rate than achievable will the full frame?
Is the 954 the best choice for a companion deserializer to the 953 serializer?
Thank you, M.Reich