This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125BR800: we want to get the configuration for 800 from the configuration of 820

Part Number: DS125BR800
Other Parts Discussed in Thread: DS125BR820,

hi team,

my customer has designed a board with DS125BR820 or DS125BR800, currently we have tested the 820, and we want to get the configuration for 800. Could you please help provide it? EQ:0x2F  VOD:0xAE  VOD_DB:0x82, Thanks.

  • Hi Frank,

    What type of configuration?  Pin levels?  EEPROM file?

    Thanks and Regards,

    Lee

  • Hi Lee,

    Any is fine, they want to achieve the same function with 800. The EEPROM is better. Thanks.

  • Hi Frank,

    Here is a low gain configuration to approximate the DS125BR820.

    Regards,

    Lee

    :2000000040001000230000000000000000000000000000000000000000000000000000006D
    :20002000000000000004070000AC00000AC00000AC00000AC0018001580000158000015801
    :20004000000015800000545400000000000000000000000000000000000000000000000063
    :20006000000000000000000000000000000000000000000000000000000000000000000080
    :20008000000000000000000000000000000000000000000000000000000000000000000060
    :2000A000000000000000000000000000000000000000000000000000000000000000000040
    :2000C000000000000000000000000000000000000000000000000000000000000000000020
    :2000E000000000000000000000000000000000000000000000000000000000000000000000
    :00000001FF
    

  • hi team,

    if the customer only use the I2C, could you please share the configuration of the register? Thanks.

  • Hi Frank,

    Here are the register writes to make the same configuration in I2C.  Register 0x06 to enable SMBus access and then 3 registers per channel to set EQ, VOD and VOD_DB.

    Address       Data

    0x06            0x18

    0x0F            0x00

    0x10            0xAC

    0x11            0x00

    0x16            0x00

    0x17            0xAC

    0x18            0x00

    0x1D            0x00

    0x1E            0xAC

    0x1F            0x00

    0x24            0x00

    0x25            0xAC

    0x26            0x00

    0x2C            0x00

    0x2D            0xAC

    0x2E            0x00

    0x33            0x00

    0x34            0xAC

    0x35            0x00

    0x3A            0x00

    0x3B            0xAC

    0x3C            0x00

    0x41            0x00

    0x42            0xAC

    0x43            0x00

    Regards,

    Lee