Part Number: DS90CF386
Other Parts Discussed in Thread: DS90C385A
Hi,
I'm using DS90CF386. I have some questions about this chip. Could you please help me?
1. The input data of the LVDS to RGB and time sequence is 1:1 or 7:1?
2. The LVDS output voltage level is 2.5V, then the input of DS90CF386 must be 2.5V or 3.3V?
3. Is there any user guide about this chip?
4. The chip will output the same data with input? or the input data must be the correct format?
Thanks.
Kevin Xiong