Part Number: DS90C187
Hi, the VOS output range of DS90C187 is is 0.8V min, 0.9V typ, 1.0V max, but we have LCD vendor requiring the LVDS signal follow below spec, looks DS90C187 output can meet the LCD spec except on the VOS, please advise if this is really a concern for interface this LCD or not? BTW, I see different LCD vendor require different on the VOS, some can reach to 0.7V min and 1.2V max, do you have experience on this why the VOS range is different between various LCD, is there a standard voltage level range in LVDS standard?