This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987EVM: Exception Error of Application Customization Tool

Part Number: TPS65987EVM

In Debug Mode,

I always encounter this message after I change any setting like below picture.

In spite of error message, I think that Setting is applied because I see modificated settings in debug mode after re-enter debug mode.

(I'm sorry that uploading picture is failed)

Exception Encountered during Drop Down Update:Internal C++ object (FixedRecordTable) already deleted.

<type 'exceptions.RuntimeError'>

Traceback (most recent call last):

File "qtRegisterClassExtensions.pyc", line 715, in drop_down_callback

File "section_widget.pyc", line 2277, in updateSectionFromDevice

File "section_widget.pyc", line 370, in updateSectionFromDeviceList

RuntimeError: Internal C++ object (FixedRecordTable) already deleted.