Part Number: UCC5606
Hello,
We are verifying this product works down to 0C and we have been seeing SCSI interface failures around this temperature. The system current begins to bounce around (~0.5A to ~0.8A) and the SCSI device is no longer detected. I am not sure the UCC5606 is at fault here but I wanted to verify our design is okay. Questions below:
- Any reason this device would not function properly around 0C? Is there an internal cold temp shutdown?
- We tie the /DISCNCT pin of each device to TERMPWR through a 0ohm resistor (Rd).
- We do not chain each /DISCNCT pin together before connecting to TERMPWR
Compare to UCC5606 datasheet pg5, figure 2.