Part Number: DS90UB954-Q1
Hi,
I'm trying to use the 954 GPIO pins for debug but am having difficulty in correlating the results.
I have GPIO pins configured to output FV and LV signals for an incoming FPD port to a remote 953
I am testing the attached sensor with varying frames sizes but have noticed that my settings do not always correlate with values signals reported by 954.
It would be helpful if you could explain the following:
1. 954 registers (0x75,76) report line count as 1080 - but the LV signal is toggling 2160 times during FV assertion.
2. 954 registers (0x75,76) report line count as 1620 - LV signal is toggling 1620 times during FV assertion.
The datasheet indicates that each long packet will be counted as a video line. If this is true it would seem that each CSI-2 long packet may only contain half the video line data.
This seems to contradict the sensor datasheet.
Can you please clarify exactly what the LV signal indicates? Does it identify video lines or packet boundaries?
Also, I'm wanting to synchronise the video streams on the each of the 953 ports of the 954.
I can configure a GPIO to indicate if synchronisation has been achieved. The output resulting signal is pulsed - does this indicate correct synchronisation or should the signal remain permanently high to indicate synchronisation.?
Thanks
Paul